:TDR:STIMulus:CHANnel:AMPLitude
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:STIMulus:CHANnel{1:8}{A|B|C|D}:AMPLitude <volts>
Where {1:8}{A|B|C|D} identifies a channel. For example, 2A. For differential channels, the alpha portion of the identifier to select from is {A|C}. For example, 1A.
Where the <volts> argument is a double.
Query Syntax
:TDR:STIMulus:CHANnel{1:8}{A|B|C|D}:AMPLitude?
Description
Sets the amplitude of the TDR stimulus step in N1055A TDR modules. The step can be set to 100 mV or 200 mV only. Any other entered value will result in the TDR step being set to the nearest value: 100 mV or 200 mV. Values entered less than 100 mV or greater than 200 mV will result in an error. Negative values are not allowed. To specify the step polarity, use the :TDR:STIMulus:CHANnel:POLarity command.
The amplitude step cannot be set on 54754A TDR modules.
Requires FlexDCA revision A.04.00 and above.
Example Command
:TDR:STIMulus:CHANnel2A:AMPLitude 200E-03