:TDR:FINCrement
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:FINCrement <frequency>
The <frequency> argument is a double.
Query Syntax
:TDR:FINCrement?
Description
For frequency-domain graphs, sets the frequency increment (separation) between adjacent data points. This setting applies to all frequency-domain graphs. This also sets the frequency separation between data points in saved S-parameter files.
Requires FlexDCA revision A.04.00 and above.
Example Command
:TDR:FINCrement 1.60E+7