:TDR:DUT:RISetime
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:DUT{1:16}:RISetime <seconds>
Where {1:16} indicates one of 16 possible DUT setups.
Query Syntax
:TDR:DUT{1:16}:RISetime?
Description
Adjust the 10% to 90% rise time of the TDR stimulus steps in seconds. The rise time should be adjusted after a TDR calibration has been completed. The setting range depends on the TDR/TDT module that is installed. Rise time is ofter used to match the stimulus step to the rise time of the actual signal that is expected to be applied to the DUT.
Requires FlexDCA revision A.04.00 and above.