:TDR:ESParameters
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:ESParameters {ON | OFF}
Query Syntax
:TDR:ESParameters?
Description
Extends the maximum measured S-Parameter stop frequency to 70 GHz on specific N1055A TDR modules identified in the following table. The extended S-Parameter range (>50 GHz to 70 GHz) in the response has no specification or characteristics, but can be informative especially when the setup has been calibrated. The measured S-Parameters can be displayed on Magnitude, Phase, and Group Delay charts. Use:TRACe subsystem commands to Select S-Parameters to view and the type of chart to display them in.
| Module Option | Extended S-Parameters Setting | |
|---|---|---|
| Off | On | |
| N1055A-32M | 35 GHz | not available |
| N1055A-32F | 35 GHz | not available |
| N1055A-34M | 35 GHz | not available |
| N1055A-34F | 35 GHz | not available |
| N1055A-52M | 50 GHz | 70 GHz 1 |
| N1055A-52F | 50 GHz | 70 GHz 1 |
| N1055A-54M | 50 GHz | 70 GHz 1 |
| N1055A-54F | 50 GHz | 70 GHz 1 |
Not specified within >50 GHz and 70 GHz extended range.
Requires FlexDCA revision A.07.60 and above.
Example Command
:TDR:ESParameters ON