:TDR:CHANnel:DUT
Command Syntax
:TDR:CHANnel{1:8}{A|B|C|D}:DUT {NONE | DUT{1:16} }
Where {1:8}{A|B|C|D} identifies a specific channel and must be selected from {1:8}{A|B|C|D}. For example, 2A. For differential channels, the alpha portion of the identifier to select from is {A|C}. For example, 1A.
Query Syntax
:TDR:CHANnel{1:8}{A|B|C|D}:DUT?
Description
Selects an enabled TDR DUT setup to which to connect the indicated channel. Up to 16 DUT setups can be enabled using the :TDR:DUT:ENABle command. If only one DUT setup is enabled, you do not need to select the DUT using the :TDR:CHANnel:DUT command. To select the DUT port to which to connect the indicated channel, use the :TDR:CHANnel:PORT command.
To successfully assign a channel to the DUT, you must use both the :TDR:CHANnel:DUT and :TDR:CHANnel:PORT commands. Or, you can have the available channels automatically selected and connected to the DUT, use the :TDR:DUT:ACONnect command.
Requires FlexDCA revision A.04.00 and above.
Example Command
:TDR:CHANnel2B:DUT DUT1