:TDR:DUT:STATus

Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter

Query Syntax

:TDR:DUT{1:16}:STATus?

Where {1:16} indicates one of 16 possible DUT setups.

Query Response

{CORR | INV | QUES}
CORR
The DUT setup is correct.
INV
The DUT setup is invalid.
QUES
The DUT setup is questionable.

Description

Queries the status of the TDR DUT setup. Use the STATus:REASon? child query to determine the reason for a invalid or questionable status.

Requires FlexDCA revision A.04.00 and above.

Child Commands