:TDR:STIMulus:SLOT:RATE:AUTomatic
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:STIMulus:SLOT{1:8}:RATE:AUTomatic {ON | OFF}
Where {1:8} identifies a module slot.
Query Syntax
:TDR:STIMulus:SLOT{1:8}:RATE:AUTomatic?
Description
Turns automatic selection of the TDR step rate on and off. By default, the rate is set to automatic. When set to manual, use the :TDR:STIMulus:SLOT:RATe command to manual enter the value.
Requires FlexDCA revision A.04.00 and above.
Command Sequence
:TDR:STIMulus:SLOT1:RATe:AUTomatic OFF :TDR:STIMulus:SLOT1:RATE 1.5E+5