:TDR:STIMulus:CHANnel:STATus?
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Query Syntax
:TDR:STIMulus:CHANnel{1:8}{A|B|C|D}:STATus?
Where {1:8}{A|B|C|D} identifies a channel. For example, 2A. For differential channels, the alpha portion of the identifier to select from is {A|C}. For example, 1A but not 1B.
Query Response
{AVA | UNAV}
Description
Queries the availability of a TDR stimulus step which is associated with the specified channel. A step becomes available (AVA) when a TDR module is installed. Otherwise, the step is unavailable (UNAV).
Requires FlexDCA revision A.04.00 and above.
Example Command
:TDR:STIMulus:CHANnel2A:STATus?