:TDR:EXPerience
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:EXPerience {BCONtrol | DCENtric}
Query Syntax
:TDR:EXPerience?
Description
Configures the TDR DUT setup user experience in the TDR Setup dialog to be DUT based (DCENtric) or basic control (BCONtrol). The DUT based user experience has the following advantages:
- Easiest to use and most Intuitive.
- Shows available S-parameters and time-domain parameters.
- Assign custom names to ports.
Requires FlexDCA revision A.04.00 and above.
Example Command
:TDR:EXPerience BCONtrol