:TDR:DUT:ADPNaming
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:DUT{1:16}:ADPNaming {ON | OFF}
Where {1:16} indicates one of 16 possible DUT setups.
Query Syntax
:TDR:DUT{1:16}:ADPNaming?
Description
Turns automatic DUT naming on Waveform content windows on or off. This determines if differential waveforms are identified in the displayed window legend by individual DUT (+/–) (OFF) or by the differential port name (ON). Use the :TDR:ASNaming command to display the window legend by channel (OFF) or by the DUT's port name (ON). The default setting is on. These settings do not affect the legend on other TDR Mode content windows.
To enter custom user labels for differential port and +/– signals, use the following commands:
- :TDR:DUT:DIFFerential:SIGNal:UNAMe
- :TDR:DUT:DIFFerential:PPORt:UNAMe
- :TDR:DUT:DIFFerential:NPORt:UNAMe
| ASNaming Command OFF | ASNaming Command ON | ||
|---|---|---|---|
| Default Port Labels |
Custom Labels | ||
| ADPNaming Command OFF (Custom Diff +/– Labels) |
ADPNaming Command ON (Custom Diff Port Labels) |
||
|
|
|
|
Requires FlexDCA revision A.04.00 and above.