:TDR:DUT:DTYPe

Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter

Command Syntax

:TDR:DUT{1:16}:DTYPe  {SEPorts{1 | 2 | 4 | 8 | 12 | 16} | DPORts{1 | 2 | 4 | 6 | 8} }

Where {1:16} indicates one of 16 possible DUT setups.

For a single-ended DUT, the argument SEPorts{1 | 2 | 4 | 8 | 12 | 16} indicates the number of ports as illustrated in the table in this topic.

For a differential DUT, the argument DPORts{1 | 2 | 4 | 6 | 8} indicates the number of ports as illustrated in the table in this topic.

Query Syntax

:TDR:DUT{1:16}:DTYPe?

Description

Selects the type of DUT to use during the TDR Setup. To select single-ended or differential ports, use the :TDR:AMODe command.

Arguments and Selected DUT
Number
of Ports
Single-Ended DUT Differential DUT
Argument DUT Argument DUT
1 SEPorts1 DPORts1
2 SEPorts2 DPORts2
4 SEPorts4 DPORts4
6 — DPORts6
8 SEPorts8 DPORts8
12 SEPorts12 —
16 SEPorts16 —

Requires FlexDCA revision A.04.00 and above.

Example Command

:TDR:DUT2:DTYPe SEPorts4