:TDR:DUT:SENDed:PORT:UNAMe
Command Syntax
:TDR:DUT{1:16}:SENDed:PORT{1:16}:UNAMe <string>
Where {1:16} indicates one of 16 possible DUT setups or DUT ports.
Query Syntax
:TDR:DUT{1:16}:SENDed:PORT{1:16}:UNAMe?
Description
Replaces the default port signal labels with custom user labels for the selected port of a single-ended DUT. The default port labels are Port 1, Port 2, …. The normal channel, default port, and custom user signal labels are displayed in the Waveform content windows as shown in the following picture. Your custom user name can include up to 25 characters. To reset a custom user label to its default port label, send an empty string.
| Normal Channel Labels | Default Port Labels | Custom User Labels |
|---|---|---|
|
|
|
To display the default port or custom user label, use the :TDR:ASNaming command. User labels (names) are helpful because they identify what a waveform represents rather than the input channel. For example, you could assign a user name "DUT Gain".
Requires FlexDCA revision A.04.00 and above.