:TDR:STIMulus:SLOT:RATE
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:STIMulus:SLOT{1:8}:RATE <frequency>
Where {1:8} identifies a module slot.
Where <frequency> is a double.
Query Syntax
:TDR:STIMulus:SLOT{1:8}:RATE?
Description
Specifies the rate, in Hertz, at which the TDR step occurs. If the stimulus rate is set to be automatically configured, entering a rate results in an error. Set the :TDR:STIMulus:SLOT:RATe:AUTomatic command to manual so that your entered rate will be applied.
Requires FlexDCA revision A.04.00 and above.
Command Sequence
:TDR:STIMulus:SLOT1:RATe:AUTomatic OFF :TDR:STIMulus:SLOT1:RATE 1.5E+5