:TDR:STIMulus:CHANnel:STEP
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:STIMulus:CHANnel{1:8}{A|B|C|D}:STEP {ON | OFF}
Where {1:8}{A|B|C|D} identifies a channel. For example, 2A. For differential channels, the alpha portion of the identifier to select from is {A|C}. For example, 1A but not 1B.
Query Syntax
:TDR:STIMulus:CHANnel{1:8}{A|B|C|D}:STEP?
Description
Turns the selected TDR stimulus step on or off.
Requires FlexDCA revision A.04.00 and above.
Example Command
:TDR:STIMulus:CHANnel2A:STEP ON