:MEASure:EYE:TDEQ:LOCation?

Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4
Optical
Electrical
Package License:
L-RND
L-MFG

Query Syntax

:MEASure:EYE:TDEQ:LOCation?

Description

Returns an index for the location of the TDEQ measurement results in the active measurement list. Using this information, you can select, clear, or remove measurement results from the displayed results table. If the measurement is not listed in the table, a "−1" is returned.

Requires FlexDCA revision A.05.60 and above.