N7841A Tests Overview

  • N7841A calibration application versions E.04.02 and greater require a minimum version of firmware to be installed in the FieldFox to successfully run tests and adjustments. Refer to the Firmware Requirements section for more information.

  • Some FieldFox model and option combinations will require the installation of the CFG Option in order to complete tests. All adjustments will require the CFG Option. Refer to the CFG Option section for more information.

The performance verification and functional tests are designed to provide the highest level of confidence that the instrument being tested conforms to published, factory-set specifications. Specifications and typicals for FieldFox analyzers can be found in the Data Sheet located on the Keysight website. Click on the Document Library tab.

Tests must be performed while the FieldFox internal temperature is within the range specified in the warm-up section. Each test will check the UUT's internal temperature sensors at the beginning and at the end of the test. The values will be included in the report.

If the analyzer is unable to pass any of the tests, then adjustments or repairs may be needed. 

Test Types

There are two types of tests: performance and functional.

The failure of either a performance test or a functional test indicates the need for adjustment or repair.

Tests by Model Number

The tests to be performed are determined by the FieldFox model number. Follow the links below for each model's list of required tests. Refer to the test page for specific model and option requirements. To expand all, click the Expand All button in the toolbar (webhelp only).

The Functional Area column in the tables below indicate if a given test applies exclusively to the NA (network analyzer) function, the SA (spectrum analyzer) function, or to both.

For N9912A , Closedclick here:

 

For N9923A , Closedclick here:

 

For all other N991xA models, Closedclick here:

 

For N991xB models, Closedclick here:

 

For all other N992xA models, Closedclick here:

 

For N993xA models, Closedclick here:

 

For N993xB models, Closedclick here:

 

For N995xA models, Closedclick here:

 

For N996xA models, Closedclick here: